init      Linker Generated Symbol File

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

init      Linker Generated Symbol File

1,955件の閲覧回数
wanglong
Contributor II

在rom.map没有这个是为什么?

ラベル(1)
4 返答(返信)

1,804件の閲覧回数
wanglong
Contributor II

Boot Assist Module (BAM) with FlexCAN MPC5534

Hello !

I need to use the Boot Assist Module to boot an application from FlexCan bust to internal SRAM.

 I  modify the start.c,but my rom.mot is not use.

Can help me with a example code? Just I have to modify the Linker Files?

Thank you very much for your time!

0 件の賞賛
返信

1,804件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Please do not duplicate the threads. Follow https://community.nxp.com/thread/443190 

0 件の賞賛
返信

1,804件の閲覧回数
wanglong
Contributor II

Hi, I met a problem when I was using mpc5634, and I generated ram.mot files on the way you provided, but my application didn't run on ram! What's the reason? Can help me? Thank you for your。

0 件の賞賛
返信

1,804件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

at first, could you please write your question in English? Second, the question does not make any sense to me. Could you please clarify it?

Regards,

Martin