how to program a binary file into MPC5674F'S internal flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program a binary file into MPC5674F'S internal flash

1,270件の閲覧回数
汶颖谢
Contributor I

I've made a binary file(*.bin) using another compiler which is compatible with the GNU, but when using the PEMICRO-jtag to download the binary into the mpc5674f's internal flash ,the tool doesn't allow me to do so by using the "DATA_LOAD" command ,I don't know what's wrong with it. I would appreciate it if anyone can explain the reason or offer me some other ways to program the binary file into the mcu's internal flash. 

NOTE: not an elf because the tool is ok with the codewarrior's elf output file.   

 

Or you can contact me through my email :[email protected] .

ラベル(1)
0 件の賞賛
返信
1 返信

1,114件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I think this is question for PEMicro. Could you please contact their support? They should be able to provide you more accurate information.

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

Regards,

Martin

0 件の賞賛
返信