freeRTOS on SDK_RTM3_0_0 for MPC574x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

freeRTOS on SDK_RTM3_0_0 for MPC574x

1,809 次查看
zhaoyanling
Contributor III

Dear expert:

I development On DEVKIT-MPC5748G board, and I use SDK_RTM_3_0_0, I have add the file path, but there is an error, shown as following. How can I resolve the problem? Can you help me?

error1.jpg

SDK_version.jpg

path.jpg

标记 (2)
0 项奖励
回复
3 回复数

1,742 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

did you generate PE code again once you added FreeRTOS component

pastedImage_1.png

The file is then located in Generate Code folder

BR, Petr

0 项奖励
回复

1,742 次查看
zhaoyanling
Contributor III

Hallo Petr Stancik,

Thank you very much for your reply.

Yes , PE codes are generated, shown as following. What may be the other reasons? 

generated.jpg

0 项奖励
回复

1,742 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

so you generated PE code, then built the project again and error still appears, weird.

Not sure, check paths, clear errors manually in Problems window, clean project and build it once again.

BR, Petr  

0 项奖励
回复