flashing with bin2hex conversion file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flashing with bin2hex conversion file

Jump to solution
1,660 Views
bjrajendra
Senior Contributor I

Hello all,

I'm using MPC5602P on CW2.9 platform. I wanted to know what will happen if I flash the unused bytes with 0x00 instead of 0xFF. The reason why I'm asking is, after my bin2hex conversion all my unused bytes are filled with 0x00 but not 0xFF. Also I don't want to use direct mot or hex file. Kindly help.

Thanks in advance,

BJ Rajendranath

0 Kudos
Reply
1 Solution
1,559 Views
bjrajendra
Senior Contributor I

Nothing happens. You can still flash with 0x00 and the code will work as expected.

View solution in original post

0 Kudos
Reply
1 Reply
1,560 Views
bjrajendra
Senior Contributor I

Nothing happens. You can still flash with 0x00 and the code will work as expected.

0 Kudos
Reply