files not found to flash while using codewarrior 10.6 version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

files not found to flash while using codewarrior 10.6 version

1,737 Views
arthivenkatasub
Contributor III

Hi,

With the codewarrior v10.6 ,while flashing code into the MPC5643L controller using debugger, a message is shown as image files not found. Whereas, the same code is flashed to the same controller using codewarrior version 2.10. I dont know where i am missing. 

 

 

Regards,

 

Arthi V

Original Attachment has been moved to: DPM_mode.zip

0 Kudos
Reply
2 Replies

1,615 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

it looks like you have incorrectly set paths in the project. Could you please share your projects to check it?

Regards,

Martin

0 Kudos
Reply

1,615 Views
arthivenkatasub
Contributor III

Hi Sir,

I have attached the example project files which i was trying to flash. Please check it. I have updated it in the question. I have also checked the path location. 

Regards,

Arthi 

0 Kudos
Reply