etpu for mpc5777c
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear:
I am using ETPU to acquire crankshaft and cam signals. I use ETPUA0 channel to acquire crankshaft signal and ETPUA1 channel to acquire cam signal. My initialization of the ETPU is as follows:
struct etpu_config_t my_etpu_config =
{
FS_ETPU_VIS_OFF /* SCM not visible (VIS=0) */
| FS_ETPU_MISC_DISABLE /* SCM operation disabled (SCMMISEN=0) */,
/* etpu_config.misc */
FS_ETPU_MISC,
/* etpu_config.ecr_a */
FS_ETPU_ENTRY_TABLE_ADDR /* entry table base address = shifted FS_ETPU_ENTRY_TABLE */
| FS_ETPU_FCSS_DIV2 /* channel filter clock source using FPSCK divider */
| FS_ETPU_CHAN_FILTER_2SAMPLE /* channel filter mode = two-sample mode (CDFC=0) */
| FS_ETPU_ENGINE_ENABLE /* engine is enabled (MDIS=0) */
| FS_ETPU_FILTER_CLOCK_DIV2 /* channel filter clock = etpuclk div 2 (FPSCK=0), see also FCSS if using eTPU2 */
| FS_ETPU_PRIORITY_PASSING_ENABLE /* Scheduler priority passing enabled (SPPDIS=0) */,
/* etpu_config.tbcr_a */
FS_ETPU_ANGLE_MODE_ENABLE /* TCR2 works in angle mode, driven by TCRCLK input and ch.0 (AM=1) */
| FS_ETPU_TCR2_PRESCALER(1) /* TCR2 prescaler = 1 (TCR2P='1-1') */
| FS_ETPU_TCR1_PRESCALER(8) /* TCR1 prescaler = 8 (TCR1P='3-1') */
| FS_ETPU_TCRCLK_INPUT_DIV2CLOCK /* TCRCLK signal is filtered with filter clock = etpuclk div 2 (TCRCF=x0) */
| FS_ETPU_TCR2CTL_FALL /* TCR2 source = fall TCRCLK transition (TCR2CTL=2) */
| FS_ETPU_TCRCLK_MODE_2SAMPLE /* TCRCLK signal is filtered using two-sample mode (TCRCF=0x) */
| FS_ETPU_TCR1CS_DIV1 /* TCR1 source using TCR1CTL divider */
| FS_ETPU_TCR1CTL_DIV2 /* TCR1 source = etpuclk div 2 (see also TCR1CS if using eTPU2) */,
/* etpu_config.stacr_a */
FS_ETPU_TCR1_STAC_SERVER /* TCR1 resource operates as server (RSC1=1) */
| FS_ETPU_TCR2_STAC_SERVER /* TCR2 resource operates as server (RSC2=1) */
| FS_ETPU_TCR1_STAC_DISABLE /* TCR1 operation on STAC bus disabled (REN1=0) */
| FS_ETPU_TCR2_STAC_DISABLE /* TCR2 operation on STAC bus disabled (REN2=0) */
| FS_ETPU_TCR1_STAC_SRVSLOT(0) /* TCR1 resource server slot = 0 (SRV1=0) */
| FS_ETPU_TCR2_STAC_SRVSLOT(0) /* TCR2 resource server slot = 0 (SRV2=0) */,
/* etpu_config.ecr_b */
FS_ETPU_ENTRY_TABLE_ADDR
| FS_ETPU_FCSS_DIV2
| FS_ETPU_CHAN_FILTER_2SAMPLE
| FS_ETPU_ENGINE_ENABLE
| FS_ETPU_FILTER_CLOCK_DIV2
| FS_ETPU_PRIORITY_PASSING_ENABLE,
/* etpu_config.tbcr_b */
FS_ETPU_ANGLE_MODE_ENABLE
| FS_ETPU_TCR2_PRESCALER(1)
| FS_ETPU_TCR1_PRESCALER(8)
| FS_ETPU_TCRCLK_INPUT_DIV2CLOCK
| FS_ETPU_TCR2CTL_DIV8
| FS_ETPU_TCRCLK_MODE_2SAMPLE
| FS_ETPU_TCR1CTL_DIV2,
/* etpu_config.stacr_b */
FS_ETPU_TCR1_STAC_SERVER
| FS_ETPU_TCR2_STAC_SERVER
| FS_ETPU_TCR1_STAC_DISABLE
| FS_ETPU_TCR2_STAC_DISABLE
| FS_ETPU_TCR1_STAC_SRVSLOT(0)
| FS_ETPU_TCR2_STAC_SRVSLOT(0),
/* etpu_config.wdtr_a */
FS_ETPU_WDM_DISABLED /* Watchdog Mode = disabled (WDM=0) */
| FS_ETPU_WDTR_WDCNT(0) /* watchdog count in microcycles */,
/* etpu_config.wdtr_b */
FS_ETPU_WDM_DISABLED /* Watchdog Mode = disabled (WDM=0) */
| FS_ETPU_WDTR_WDCNT(0) /* watchdog count in microcycles */
};
The ETPU CLK is 80MHz。 So we can get tcr1_freq and tcr2_freq as:
uint32_t etpu_a_tcr1_freq = 10000000;
uint32_t etpu_a_tcr2_freq = 10000000;
uint32_t etpu_b_tcr1_freq = 10000000;
uint32_t etpu_b_tcr2_freq = 10000000;
If I keep the above configuration.I can correctly capture the cam signal, but not the crank signal.If I change FS_ETPU_ANGLE_MODE_ENABLE to FS_ETPU_ANGLE_MODE_DISABLE.The crank signal can be acquired correctly.However,i need angular clock.Please give me some help and advice, thank you sincerely.
respectly
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
If you are using the angle mode configured by "FS_ETPU_ANGLE_MODE_ENABLE" the crank signal must be input via the TCRCLKA pin, not the ETPUA0 pin. Note that there are some small advantages on MPC56xx and MPC57xx devices of processing angle mode via eTPU channels 1 or 2, rather than 0. Here is some information from the MPC5777C reference manual: