when I use RAppID Boot Loader Utility to dowload application. there is message is as attached picture.
on target board side, use eSCI_A as boot serial . EVTO PIN is float. Bootcfg set as 01.
the error message told that we should use CAN interface not serial(232) interface. In fact, we used uart (232) not CAN inteface.
Would you please help to check it ?
Hello Alex,
Just to better understand your setup:
Have you downloaded .rbf file into your board first via JTAG?
RAppid BL does not support BAM "Hardware boot" for MPC57xx so BAM setup has no effect whatsoever.
Which board are you targetting - custom one of NXP EVB?
Stan