about nexus data trace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about nexus data trace

1,725 Views
whagiew
Contributor II

hi,

 I want to get the sampling data of AD in real time. Can I transfer the data in real time through the NEXUS interface? How should the host computer accept it? How can I operate the NEXUS interface? Thank you.

best regards.

 Yang

0 Kudos
Reply
2 Replies

1,600 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

what do you want to do exactly? What is the use case? I don’t think that Nexus is the right interface for you. It looks like some fast and standard communication interface (CAN or whatever) would be suitable for you.

More information about Nexus tools from Lauterbach can be found in this application note:

https://www.nxp.com/docs/en/application-note/AN4591.pdf

Regards,

Lukas

0 Kudos
Reply

1,601 Views
whagiew
Contributor II

Thank you for your reply, I want to send a lot of data, there may be 800M in one second. The R274's Zipwire is only 320M. I found that there are 4 LVDS interfaces in Nexus Aurora, which is fast. But I have never used it, so ask for help here.

Regards,

Yang

0 Kudos
Reply