ZipWire SW information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZipWire SW information

3,259件の閲覧回数
rajkumarkk
Contributor I

Dear All,

 I am working with ZipWire for communication between 2 MPC5777C controllers,

for make the synchronization of PWM signals generated by the ETPU module.

It would be helpful if have any SW information is available regarding the ZipWire communication in MPC5777C

Thanks all

With Regrads

Rajkumar

5 返答(返信)

2,635件の閲覧回数
alanwu
Contributor I

Would you send the sample code with AN5134 to my email? The link on NXP.com is invalid. Thank you.

0 件の賞賛
返信

3,130件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have already send you requested examples + pdf presentation via separate email.

Peter

3,044件の閲覧回数
yangjieyong
Contributor I
Dear Peter, Could you also send me a copy of the two SPC5777C communication routines via Zipwire, together with the corresponding PDF documents?If there is the ability to achieve network port, serial port message routing is better.Thank you very much.
0 件の賞賛
返信

3,130件の閲覧回数
rajkumarkk
Contributor I

Hi Peter,

Thanks for your support and will get back to you if need any more information or quires later

Hence you can close this ticket

With Regards,

Rajkumar K

0 件の賞賛
返信

3,130件の閲覧回数
lucabarbiero
Contributor IV

Hi Raijkumar,

Did you manage to use the Zipwire to synchronize PWMs generated by eTPU modules in two different MPC5777C? I am just looking into this now. Was this successful? What challenges did you face? Any hint would be much appreciated!

petervlna‌ i would like to receive all existing supporting information as well. Should I open a formal ticket?

Regards,

Luca 

0 件の賞賛
返信