Which channels of the ETPU cannot be used as PWM input in MPC5634

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which channels of the ETPU cannot be used as PWM input in MPC5634

ソリューションへジャンプ
1,925件の閲覧回数
ZEROOO
Contributor IV

Hi

  When I configured eTPU27 channel as PWM input in MPC5634,I found the IPS bit in SCR register of eTPU27 was 0 all the time.The CHIP manual indicates that eTPU27 has IO function,when select PA.However, the PWM input is not detected through debugging monitoring.The ETPU reference manual is found in the second picture,in which I found that ETPU was not connected with Pin.Why is the chip reference manual different from the ETPU manual?Are there differences in understanding between the two places?Does this etpu manual apply to other MPC5XXX chips?Please reply the soonest possible.

    Best wishes!

ZEROooo_0-1653699246445.png

ZEROooo_1-1653699431304.png

 

 

 

0 件の賞賛
返信
1 解決策
1,877件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It seems screenshot from eTPURM is only related MPC55xx device where eTPU modules is used. MPC56xx use eTPU2 module.

I guess you forgot setup below:

davidtosenovjan_2-1653917679529.png

davidtosenovjan_1-1653917601376.png

 

元の投稿で解決策を見る

4 返答(返信)
1,860件の閲覧回数
ZEROOO
Contributor IV

Thank you very mush.I want to know that someone sent me this ETPURM screenshot. Where can I find it.Can you tell me where to look for the difference between ETPU and ETPU2?

0 件の賞賛
返信
1,853件の閲覧回数
johndiener
Contributor IV

The eTPU2 reference addendum can be found at https://www.nxp.com/files-static/32bit/doc/ref_manual/ETPURMAD.pdf.

John Diener
1,878件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It seems screenshot from eTPURM is only related MPC55xx device where eTPU modules is used. MPC56xx use eTPU2 module.

I guess you forgot setup below:

davidtosenovjan_2-1653917679529.png

davidtosenovjan_1-1653917601376.png

 

1,851件の閲覧回数
ZEROOO
Contributor IV

Thank you very much.Can you tell me where to look for the difference between ETPU and ETPU2?Where can I find the ETPURM manual and this screenshot was sent to me.

0 件の賞賛
返信