Which channels of the ETPU cannot be used as PWM input in MPC5634

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which channels of the ETPU cannot be used as PWM input in MPC5634

Jump to solution
1,858 Views
ZEROOO
Contributor IV

Hi

  When I configured eTPU27 channel as PWM input in MPC5634,I found the IPS bit in SCR register of eTPU27 was 0 all the time.The CHIP manual indicates that eTPU27 has IO function,when select PA.However, the PWM input is not detected through debugging monitoring.The ETPU reference manual is found in the second picture,in which I found that ETPU was not connected with Pin.Why is the chip reference manual different from the ETPU manual?Are there differences in understanding between the two places?Does this etpu manual apply to other MPC5XXX chips?Please reply the soonest possible.

    Best wishes!

ZEROooo_0-1653699246445.png

ZEROooo_1-1653699431304.png

 

 

 

0 Kudos
Reply
1 Solution
1,810 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It seems screenshot from eTPURM is only related MPC55xx device where eTPU modules is used. MPC56xx use eTPU2 module.

I guess you forgot setup below:

davidtosenovjan_2-1653917679529.png

davidtosenovjan_1-1653917601376.png

 

View solution in original post

4 Replies
1,793 Views
ZEROOO
Contributor IV

Thank you very mush.I want to know that someone sent me this ETPURM screenshot. Where can I find it.Can you tell me where to look for the difference between ETPU and ETPU2?

0 Kudos
Reply
1,786 Views
johndiener
Contributor IV

The eTPU2 reference addendum can be found at https://www.nxp.com/files-static/32bit/doc/ref_manual/ETPURMAD.pdf.

John Diener
1,811 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It seems screenshot from eTPURM is only related MPC55xx device where eTPU modules is used. MPC56xx use eTPU2 module.

I guess you forgot setup below:

davidtosenovjan_2-1653917679529.png

davidtosenovjan_1-1653917601376.png

 

1,784 Views
ZEROOO
Contributor IV

Thank you very much.Can you tell me where to look for the difference between ETPU and ETPU2?Where can I find the ETPURM manual and this screenshot was sent to me.

0 Kudos
Reply