Version Difference between MPC5606BK and MPC5606BF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Version Difference between MPC5606BK and MPC5606BF

1,458 Views
JohnnyChen
NXP Employee
NXP Employee

 

MPC5606/5BK are derivatives of Bolero1M device while MPC5607/6/5BF are derivatives of Bolero1.5M device.

 

MPC5606BK datasheet:

http://cache.freescale.com/files/32bit/doc/data_sheet/MPC5606B.pdf

MPC5607BF datasheet:

http://cache.freescale.com/files/32bit/doc/data_sheet/MPC5607B.pdf

 

Following Bolero versions exist:

  Name Family Cut mask
1 MPC5606/5BK BOLERO_1M 1.0 0N13E
2 MPC5607/6/5BF BOLERO1_5M 1.0 0M94V
3 MPC5607/6/5BF BOLERO1_5M 2.0 0M03Y
4 MPC5607/6/5BF BOLERO1_5M 2.2 1M03Y
5 MPC5607BK BOLERO1_5M 2.2 0N69H

 

Questions:

A: (4) is identical to (5); only difference is manufactured in different factory. Is it right?

- Yes, it is. Even content of errata sheets is equal.

 

B: (3) is different to (4),(5). Whats the difference between cut2.2 and cut2.0?

- There are different errata between these revisions:

http://cache.freescale.com/files/32bit/doc/errata/MPC5607B_0N69H.pdf

http://cache.freescale.com/files/32bit/doc/errata/MPC5607B_1M03Y.pdf

http://cache.freescale.com/files/32bit/doc/errata/MPC5607B0M03Y.pdf

 

MPC5607BK and MPC5607BF are being manufactured in different facility, thats why they have different mask although cut number (i.e. revision) is the same.

 

C: Whether SPC5607BK 144LQFP is pin compatible with SPC5606BF 144LQFP?

- Yes, all variants are pin-to-pin compatible to each other.

 

We know that there are minor updates and difference between SPC5606BK and SPC5606BF which is mentioned in AN4477. Does it the same to SPC5607BK and SPC5607BF?

- No, it is not the same. AN4477 describes difference between Bolero1.5M and Bolero1M.

- SPC5607BK and SPC5607BF are both derivatives of Bolero1.5M, should follow MPC5607B.pdf, MPC5607BRM.pdf

 

0 Kudos
Reply
0 Replies