Using EMIOS0 is to capture or PWM for different cycles

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using EMIOS0 is to capture or PWM for different cycles

2,875 次查看
thomasbao
Contributor II

hello, everyone:

    I want to use eMIOS_0[13] generate PWM(30 ms), and to use eMIOS_0[12] as input capture in interrupt mode(120 ms). How should it to be implemented?

标记 (2)
0 项奖励
回复
3 回复数

2,865 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to emios demo example within S32DS and modify it per your need

PetrS_0-1629789237793.png

 

BR, Petr

 

0 项奖励
回复

2,861 次查看
thomasbao
Contributor II

Hi Petr,

    Thank you for your reply. And I wonder if I can implement this feature directly using the SDK ?

0 项奖励
回复

2,858 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, the SDK driver can be used as well and "ic", "pwm" examples are available too

PetrS_0-1629800521359.png

 

BR, Petr

0 项奖励
回复