Unable to write in EEPROM Memory.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to write in EEPROM Memory.

3,935件の閲覧回数
Balakrishna24
Contributor I

Hi, 

I am trying to access and modify boot code EEPROM emulation in mpc5746c microcontroller.

I am not able to write in the boot code EEPROM memory. 

I have took example project EEPROM emulation in S32 design studio. 

I am getting IVOR6 Program exception. I hope someone can answer this question. 

 

Thanks.

0 件の賞賛
返信
3 返答(返信)

3,879件の閲覧回数
Balakrishna24
Contributor I

Hi @lukaszadrapa 

code is running from Start Address is 0x00F90000 and Block size is 0x00004000.

Flash Start Address is 0x00F90000.

No, i didn't check the details in register as you mentioned.

 

Thanks.

0 件の賞賛
返信

3,843件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Does it mean that the code is running from the block which is being erased?

In default example, the code is running from large blocks (0x0100_0000) and these blocks are used for EEE:

lukaszadrapa_0-1730729375947.png

 

0 件の賞賛
返信

3,892件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Balakrishna24 

which block is being erased exactly? Where the code is running from?

Did you check the details about IVOR6 exception?

lukaszadrapa_0-1730448213179.png

Regards,

Lukas

0 件の賞賛
返信