Trigger for SDADC at MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Trigger for SDADC at MPC5777C

378 次查看
JH11
Contributor I

Hello, 

There is something I don't understand while looking at the manual.

The TRIGSEL register selects which input will be used for hardware triggered conversations

In Table 29-2, if the register is set to 0, the trigger for sdadc1 is written as reserved.

So how does the hardware trigger on sdadc1 work in this case?

Additionally, TRIGEN is set to 1.

0 项奖励
回复
1 回复

368 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Theoretically it can lead in unpredictable results but in practice it does not trigger SDADC module.

Btw I made an example for this:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-SDADC-eTPU-triggered-GHS714/ta-...

 

0 项奖励
回复