Trace32 mpc5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace32 mpc5777C

838件の閲覧回数
Othmane1
Contributor II

Hi,

I'm using Lauterbach Trace32 to debug my code for MPC5777C evaluation board, when i use one of their example to flash my elf file it flashes ok, but the moment i start stepping the code suddenly run by itself and when i check i found that some interrupts happen in the startup code (as shown in the picture below) even though my code works well when i debug it with S32 design studio, can someone help me?

I attache also the Trace32 script example i'm using.

 

Othmane1_0-1698156123347.png

 

0 件の賞賛
返信
1 返信

827件の閲覧回数
rweiss
Contributor V

This might be a FLE vs. VLE issue. Did you reset the processor (SYStem.Up) after programming the FLASH? You need to reset the processor in order to run through the boot ROM, which will set up the TLBs according to the RCHW.

0 件の賞賛
返信