The ethernet communicates with the uart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The ethernet communicates with the uart

547 Views
lixu
Contributor II

Dear everyone,

I am using S32DS working on MPC5748G.

I used the project in example to debug the network interface for communication, and I did the project of uart communication.

Now I want to send the data using the network port and then return the data through uart. May I ask if there is any relevant project or material you can draw lessons from?

Thanks and best regards,

Li Xu

0 Kudos
Reply
1 Reply

541 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

 these are the examples we have, all are included in S32 Design Studio:

 c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\lwip\

 c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\demo_apps\usb_cdc_lwip\

 c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\driver_examples\communication\enet_ping\

 c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5748G\driver_examples\communication\phy_autoneg\

 Documentation can be found here:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\doc\S32SDK_MPC5748G_UserManual.pdf

 Notice that lwip stack is not our product. If more details are needed (see external links):

https://en.wikipedia.org/wiki/LwIP

 

Regards,

Lukas

 

 

 

0 Kudos
Reply