TRK-MPC5606B flash programming with RAppId Boot Loader Utility fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TRK-MPC5606B flash programming with RAppId Boot Loader Utility fails

2,950件の閲覧回数
smorgenstern
Contributor I

Hello,

I tried to flash the evaluation board TRK-MPC5606B as described with the RAppId Boot Loader Utility, but for some reason it doesn't work.

External power 12VDC, Jumper settings (SBC_5V, J17 1-2, J18 2-3, J7 1-2, J8 1-2) as described in the corresponding training manual.

Settings: Serial Port, COM9 verified in Device Manager, baud rate 9600

BAM Status: enabled, default password

That's the first discrapency with the description because it says password 0xFFFFFFFFFFFFFFFF, but if I am using this the communication stops right away with any of these messages: "Loss Communication with BAM at Start Address. Timeout ...", or "Initialization Error with BAM. Check Password or Verify Boot Configuration Setting ABS2=1, ABS1=0, FAB=1. Please cycle power and try again."

If I am using the "default password" the boot loading at least proceeds and seems to work (progress indication increases "BTL 0% to BTL 100 %" then "Init") but then I get the following error message "Loss Communication with CCP MCU. Please cycle power and try again. Timeout ...".

I get the same results also when I attempt to flash the delivered example files "Training_LED_Example.mot" or "FSK_LED_Example.mot" (code range "auto read").

 

Any help appreciated. Regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,834件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I have tested the RAppID bootoader on my TRK-MPC5606B board and it works well. Attached is the test example I used. It just toggle a LED1.

Here are few points you should keep…

- you have to select proper COM port as it is assigned to a CDC Serial Port in PC’s Device Manager

- the TRK-MPC5606B contains the MPC5606BK device, so this one should be selected in RAppID BL tool.

Note the MPC5606BK has 0N13E mask, while MPC5606B has 1M03Y mask.

- if using just the USB to power a board (USB_5V on POWER_SELECT jumpers) once a RAppID bootloader ask for cycle MCU power just the RESET button should be pressed, then press OK on RB tool window. The RESET button can be used also for other power options for sure.

- if you did not change password in the shadow flash then “Default Password” option should be selected with BAM status option “Enabled”

Hope it helps.

Regards,

Petr

0 件の賞賛
返信

1,834件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Stephan,

The Rappid is handle by a specific team which can be contacted by email: [email protected].

I don't know exactly if the question must be handle by Rappid Team or Hardware.

I recommend you to contact the Rappid Team to have their feedback.

On my side I will move the question to Hardware team.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信