TRK MPC5604B Qorivva USB power light blinking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TRK MPC5604B Qorivva USB power light blinking

1,390 Views
BhargavaVenkate
Contributor I

Hi, the green USB power light on my TRKMPC5604B was blinking a while before, and I was not able to upload code onto the board because the computer wasn't recognizing it.

The problem solved itself after we kept trying but, does anyone why it happened and how we can take solve it if it happens again?

Thanks!

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,190 Views
ioseph_martinez
NXP Employee
NXP Employee

Rather than the board itself sounds like the USB cable was not doing proper contact or even some short and the USB port on the computer was shutting down for safety. I would recommend to verify connections and make sure your bench is free of metal that can cause any shortcuts.