Synchronizing two emios modules on MPC5604B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Synchronizing two emios modules on MPC5604B

1,696件の閲覧回数
yuyangliu
Contributor I

Hi,

I am considering using MPC5604B for an application where lots of pulsed outputs are needed. And all the pulses needs to be timed on a single timer.

I understand that MPC5604B has two separate EMIOS timer modules and in the reference manual, it is briefly mentioned that the two modules can be synchronized. I would like to know how I can synchronize the two Emios modules.

For example, if I want ALL the channels in the two modules to be timed onto a single BUS A, do I need only to configure the channel 23 of emios0 and all channels in emios1 would automatically be on bus A of emios0? Or do I need to configure both channel23 of both modules? But in that case, how do I make sure both modules are totally in synch?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,593件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

counter buses are not shared between eMIOS modules. You can just enable internal counters at the same time using GTBE bit. So for example configure channel 23 on both eMIOS modules for the same setting and as last step set MCR[GTBE] of one module (on second GTBE is cleared for sure). Both counters will start at same time and so counter buses A will be synchronized.

BR, Petr

0 件の賞賛
返信

1,593件の閲覧回数
yuyangliu
Contributor I

Understood. Thank you very much!

0 件の賞賛
返信