Software development IDE and Compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Software development IDE and Compiler

2,700 Views
Eashwar
Contributor I

Hi,

I am in process of selecting one suitable processor from MPC57xx or MPC56xx or MPC55xx series for my automotive application. Also, I am new to automotive processor application of NXP. So I have few clarification on software development tools for processor mentioned in above series,

1. Are low level drivers available like BSPs? Is there a software to generate drivers as I enable the required peripheral like in MCUXpresso?

2. Kindly list out supported IDE and compiler?

3. Is the IDE and compiler licensed or not? If paid, kindly list out cost details.

Kindly provide above details ASAP.

0 Kudos
Reply
5 Replies

2,688 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

. Are low level drivers available like BSPs? Is there a software to generate drivers as I enable the required peripheral like in MCUXpresso?

Yes, there is SDK and processor expert in S32DS for MPC5xxx family.

There are also AUTOSAR MCAL drivers free from NXP.

2. Kindly list out supported IDE and compiler?

S32DS: it is project manager, bebug host and also includes compiler (gcc) all free from NXP.

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

Besides those you can use Greehills, Windriver and some others which I don't use.

3. Is the IDE and compiler licensed or not? If paid, kindly list out cost details.

S32DS is free and it is NXP product. Any other you need to discuss with product vendor.

 

Best regards,

Peter

0 Kudos
Reply

2,686 Views
Eashwar
Contributor I

Hi Peter,

Thank you for your response and solution.

I found there is code warrior for eTPU software . I need to use eTPU functions, do I need purchase Code Warrior or is the same available in S32DS?

Regards,

Eashwar

0 Kudos
Reply

2,675 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

If you want to develop your own eTPU functions then you need to buy eTPU CW10.3 from NXP or whole development studio from Ashware.

In S32DS there is no eTPU configurator.

If you dont want your own functions, then it is enought to get functions written by NXP from eTPU function selector:

https://www.nxp.com/webapp/etpu_cw/

In this case you are not able to change eTPU code and you can only use our functions.

Best regards,

Peter

 

 

0 Kudos
Reply

2,665 Views
Eashwar
Contributor I

Dear Peter,

 

Sorry for late response. I would like to discuss my requirements in details with you. So, can we have this conversation in private (one to one) via your official mail ID.

 

Regards,

A Eashwar

 

0 Kudos
Reply

2,643 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

No. Community is public.

But you can have it private if you submit a ticket at nxp.com or if you contact NXP FAE/sales assigned to your company in case you have one.

Best regards,

Peter

0 Kudos
Reply