Shadow Flash direct programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Shadow Flash direct programming

1,990件の閲覧回数
jeffcampbell
Contributor III

Quick question - I'm attempting to alter shadow flash (fully aware of the risks; I've successfully done it already and am experimenting with the process).  Is it possible to edit the shadow block directly during the process of programming the chip (i.e. have a defined data section that gets loaded directly to Shadow Block A alongside the rest of the main program), or can it only be modified by a function executing from RAM?

ラベル(1)
0 件の賞賛
返信
1 返信

1,856件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is possible, if particular programmer have defined programming algorithm for shadow flash (for instance PeMicro debugger have them prepared …\pemicro\algorithms\shadow\).

Production programmers should be capable to do it as well as it can be just a requirement to set up censorship during production programming.

0 件の賞賛
返信