Setting IP in MPC5748G LCEVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting IP in MPC5748G LCEVB

1,785 Views
rahulramakrishn
Contributor III

Hi

In my project I need to send data from one board to the MPC5748G LCEVB board. In order to send the data I need to set the IP address for both the device. How can I configure Ethernet in MPC5748G LCEVB so that I can able to set the IP address? Is there any example projects available? 

0 Kudos
Reply
2 Replies

1,607 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I sent you the answer in the thread below:

https://community.nxp.com/thread/480417 

Regards,

Martin

0 Kudos
Reply

1,607 Views
rahulramakrishn
Contributor III

Ok. Thank you for support.

0 Kudos
Reply