SPI initial with two masters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI initial with two masters

1,068件の閲覧回数
supra0309
Contributor I

Hi :

If I want to initial both of configurations in same SPI_pal, how should I do the initialize step contemporary?

Please help me to figure out them, thanks.

BR,

Xantia

supra0309_0-1661411780764.png

supra0309_1-1661411780772.png

supra0309_2-1661411780715.png

supra0309_3-1661411780654.png

supra0309_4-1661411780652.png

0 件の賞賛
返信
1 返信

1,057件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

no, it is not possible to have both initialized in the same time for the same module.
If you want to do communication with second configuration, you need to first finish previous communication, call Deinit and then Init with new master configuration. Then you can do a communication again.

BR, Petr

0 件の賞賛
返信