SPC5744PFK1AMLQ9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPC5744PFK1AMLQ9

1,815 次查看
muthukrishnanp
Contributor II

Hi ,

We have face issue RESET Pin is Pulled low always @10K Pull up Resistor.

Pull up resistor we modified 4k7 and 3k3 values still it is pull low.there after 100E resistor used for pull up

now RESET Pin Voltage is 0.7V. What is the actual current need RESET Pin during Power on restet and debugging mode. Data sheet defined 15mA. 3.3V and 100E pull up resistor is sufficient still voltage drop persist.

any recommendation is need for RESET Pin.

Regards

Muthukrishnan P

标签 (1)
0 项奖励
回复
2 回复数

1,694 次查看
muthukrishnanp
Contributor II

Hi Thank you for the support. We have solved the issue .

Regards

Muthukrishnan P

0 项奖励
回复

1,694 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You can find recommendation in Hardware design guide:

https://www.nxp.com/docs/en/application-note/AN5267.pdf 

Both RESET_B and EXT_POR_B are open drain, active low, bidirectional pins with internal weak pull down resistors. An external 4.7 kΩ - 10 kΩ pull up resistor should be added to these pins. A simplified  diagram of RESET_B and EXT_POR_B is shown below.

pastedImage_1.png

Peter

0 项奖励
回复