SPC5741P and SPC5744P Controller Pinout is same?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5741P and SPC5744P Controller Pinout is same?

2,164件の閲覧回数
muthukrishnanp
Contributor II

Hi,

Please confirm the 32BIT Controller Pinout is pin to pin same SPC5741P and SPC5744P?

Regards

Muthukrishnan P

0 件の賞賛
返信
3 返答(返信)

1,941件の閲覧回数
muthukrishnanp
Contributor II

Hi Martin,

 

Thank you for support.

We have face issue RESET Pin is Pulled low always @10K Pull up Resistor.

Pull up resistor we modified 4k7 and 3k3 values still it is pull low.there after 100E resistor used for pull up

now RESET Pin Voltage is 0.7V. What is the actual current need RESET Pin during Power on restet and debugging mode.  Data sheet defined 15mA. 3.3V and 100E pull up resistor is sufficient still voltage drop persist. 

any recommendation is need for RESET Pin.

0 件の賞賛
返信

1,941件の閲覧回数
muthukrishnanp
Contributor II

Hi Martin,

Thank you for support.

We have face issue RESET Pin is Pulled low always @10K Pull up Resistor.

Pull up resistor we modified 4k7 and 3k3 values still it is pull low.there after 100E resistor used for pull up

now RESET Pin Voltage is 0.7V. What is the actual current need RESET Pin during Power on restet and debugging mode.  Data sheet defined 15mA. 3.3V and 100E pull up resistor is sufficient still voltage drop persist. 

any recommendation is need for RESET Pin.

0 件の賞賛
返信

1,941件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, there is the same pinout for MPC5744P and MPC5741P.

Regards,

Martin

0 件の賞賛
返信