SPC5606BF1MLQ6 CAN1 Low Power Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPC5606BF1MLQ6 CAN1 Low Power Issue

882 次查看
dannydeng
Contributor III

Dears,

  I built the project which used CAN1module, I need to let CAN1 go to low power model, that I set the TX, RX port to GPIO model. However, I found when set CAN1 to GPIO, then delay some millisecond, after that set CAN1 to Freese/Disable model, go to sleep, the current can low to 3mA. And, if set CAN1 to GPIO, set CAN1 to Freese/Disable model, delay some milesecond, then sleep, the current reach to 26mA. I found the RX_ERROR_COUNTER cannot be cleared, it is 129.

  Can anybody help to advice?

Thanks, 

Ray Deng 

0 项奖励
回复
0 回复数