SPC5605B SPI read RX problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5605B SPI read RX problem?

1,687 Views
wuxuliang
Contributor II

 CW2.10,attatchments are project  software files.At the end of main.c , I find some SPI -read ing debug errors about breakpoint position setting.

When debuging breakpoint sets at 1st breakpoint,RX is OK,and Oscilloscope observation waveform is the correct output。

 

When debuging breakpoint sets at 2nd breakpoint,RX is error,and Oscilloscope observation waveform is the correct output。

 

I want to know if there are some errors about SPI init?

Original Attachment has been moved to: main.c.zip

Original Attachment has been moved to: Project_1(SPI)---read(遗留问题).zip

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,510 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please clarify, where did you have breakpoints placed during debugging?

Regards,

Martin

0 Kudos
Reply