SENT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SENT

3,416 Views
kentsun
Contributor II

on MCU MPC5744P, I need SENT module software driver,thanks.

0 Kudos
Reply
4 Replies

3,248 Views
mvogtmann
Contributor I

I've found an old configurator for getting a SENT Driver

See in the Application Note and the file.

I have problems with getting the Makro running with Excel 2010. Is there a newer version of the Macro available?

https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fapplication...

https://www.nxp.com/docs/en/application-note/AN4856.pdf 

0 Kudos
Reply

3,248 Views
mvogtmann
Contributor I

Hello,

There was an application note describing the SENT interface and referring to an Excel-Makro sheet, which generates a driver with all necessary .h and .c-files. I couldn't find it anywhere on the Internet. It would be great if NXP could provide it again with a good demo example in S32 Studio.

Here's snapshot of the Document:

NXP_Sent_Driver.png

0 Kudos
Reply

3,248 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have asked responsible persons and

looks like we do not offer SENT driver for MPC5xxx in SDK neither in AUTOSAR.

regards,

Peter

0 Kudos
Reply

2,818 Views
ChenBowen
Contributor II

Hi, Do you have a SENT example project for MPC5744P now?

0 Kudos
Reply