Register protection mechnism

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Register protection mechnism

625 Views
abdelrhman
Contributor III

For MPC5744p, I noticed that the register protection mechanism is not provided to all the modules

what are the modules provided by register protection mechanism?

0 Kudos
Reply
2 Replies

603 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, you may find it in the RM, Appendix A

davidtosenovjan_0-1654262116768.png

 

Tags (1)
0 Kudos
Reply

609 Views
egeonurg
Contributor III

Register protection
The System Integration Unit Lite2 uses the Register Protection Scheme to protect the
individual registers from accidental writes. The following registers can be protected:
• SIUL2 DMA/Interrupt Request Enable Register 0 (SIUL2_DIRER0)
• SIUL2 DMA/Interrupt Request Select Register 0 (SIUL2_DIRSR0)
• SIUL2 Interrupt Rising-Edge Event Enable Register 0 (SIUL2_IREER0)
• SIUL2 Interrupt Falling-Edge Event Enable Register 0 (SIUL2_IFEER0)
• SIUL2 Interrupt Filter Enable Register 0 (SIUL2_IFER0)
• SIUL2 Interrupt Filter Maximum Counter Register (SIUL2_IFMCR0 to
SIUL2_IFMCR31)
• SIUL2 Interrupt Filter Clock Prescaler Register (SIUL2_IFCPR)
• SIUL2 Multiplexed Single Configuration Register (SIUL2_MSCR0 to
SIUL2_MSCR511 and SIUL2_IMCR0 to SIUL2_IMCR511): Only the specific
MSCRs and IMCRs that are actually implemented on a device are protected.
A compiled list identifies the protected registers at specific addresses for this device.

MPC5744P Reference Manual, Rev. 6, 06/2016 - 16.1.3 Register protection 

 

Regards 

Ege

 

0 Kudos
Reply