Regarding debug in core 0 and core 1 in MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding debug in core 0 and core 1 in MPC5777C

1,268 Views
sourabhjain
Contributor III

Hi i want to know that if i debug both core 0 and core 1 in MPC5777C then if i fully run or i put core 0 in Run mode and try to debug core 1 in step. Then if suppose any interrupt which is define in both core is raised in core 1 during debug ?

means we can run core 1 code with core 0 code in full run mode ?  

1 Reply

1,161 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

If the interrupt is configured to be executed in both cores, then it will be executed in both cores.

There is one interrupt controller INTC which sends external interrupt request to both cores.

The interrupts routines will be executed based on core status. (if he core is halt by debugger, then interrupt will be executed when core starts executing instructions again).

Peter