RAppID BL Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID BL Tool

Jump to solution
6,001 Views
ahmetsaglam
Contributor I

 

Hi, @mariuslucianand 

Who from NXP can help us with the open-source codes of the RApID bootloader program? We want to install software via RAppId with PCAN.

We spoke to Vector and they reported that it has been discontinued for CanCase Xl.

ahmetsaglam_0-1638885938573.pngahmetsaglam_0-1638885938573.png

 

Best Regards.

 

0 Kudos
Reply
1 Solution
5,943 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

On the RAppID BL application, please choose "Vector CANCaseXL".

Regards,

Lukas

View solution in original post

0 Kudos
Reply
5 Replies
5,034 Views
nailgg
Contributor I

Hi,

 

I also needed to use the RAppID BL software with my PCAN adapter. Slightly modified the RAppID_BL.exe to make it work with PCAN, binary can be found in the attachment. The app thinks it's Vector so Vector CANCaseXL must be chosen, but it actually sends the messages to the Peak adapter.

 

I needed this to test to see whether my SPC560P50 will work with the bootloaders in this software. I tried MPC5604/3P, it successfully uploads the BL but then it gets stuck in the Initialization phase for some reason. Been trying to figure out why for a few days but I think I'll give up so I hope this at least works for someone else.

 

0 Kudos
Reply
5,983 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ahmet,

Rappid bootloader is not an open source, we do not provide the source codes due to legal reasons.

Even if Vector tools are discontinued, we confirmed that new VN16xx tools from Vector are compatible and those can be used with Rappid bootloader.

Regards,

Lukas

0 Kudos
Reply
5,682 Views
setsaillove
Contributor I

Hello :

I do not know how to get the RAppID BL Tool.

could you please share the download address about RAppID BL Tool?

0 Kudos
Reply
5,960 Views
ahmetsaglam
Contributor I

Hi @lukaszadrapa 

We have a Vector-VN1630.

We made Vector hardware configuration.
But we can't see Vn1630 in the program. Which one should we choose?

ahmetsaglam_0-1639065903111.pngahmetsaglam_0-1639065903111.pngahmetsaglam_1-1639065954816.pngahmetsaglam_1-1639065954816.png

Regards

0 Kudos
Reply
5,944 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

On the RAppID BL application, please choose "Vector CANCaseXL".

Regards,

Lukas

0 Kudos
Reply