Questions about FLEXCAN_DRV_InstallEventCallback warning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about FLEXCAN_DRV_InstallEventCallback warning

1,144件の閲覧回数
Sang-Hoon_Ahn
Contributor I

hi
I am writing a CAN FD communication firmware utilizing the MPC5748G.

During the development of the firmware, I am using the FLEXCAN_DRV_InstallEventCallback function to write in interrupt format as much as possible.

This function takes 3 parameters as arguments, and for the callbackParam argument, I usually enter the value as 'NULL' in other examples.

ex) FLEXCAN_DRV_InstallEventCallback(INST_CANCOM1, FlexCan_RxTx_Callback, NULL);

This will cause the following warining in the function.
'passing argument 2 of 'FLEXCAN_DRV_InstallEventCallback' from incompatible pointer type'

Why does this warning occur, and can I ignore it?

0 件の賞賛
返信
1 返信

1,129件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

maybe your callback function has different parameter type used. Did you define function as below?

void FlexCan_RxTx_Callback(uint8_t instance, flexcan_event_type_t eventType, uint32_t mb_num,
flexcan_state_t *flexcanState)
{
     (void)flexcanState;
     (void)instance;

     switch(eventType)
     {
        ....

BR, Petr

0 件の賞賛
返信