Question about the MPC5748G ULPI0_Data interface output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about the MPC5748G ULPI0_Data interface output

Jump to solution
3,276 Views
H-chips
Contributor III

Dear NXP Community,

  When I used the USB0 interface of MPC5748G, after enabling the clock and interface, I used the oscilloscope to detect the potential of ULPI0_Data[0:7] as follows:

ULPI0_Data[0]: 3.3v
ULPI0_Data[1]: 0v
ULPI0_Data[2]: 3.3v
ULPI0_Data[3]: 0v
ULPI0_Data[4]: 0v
ULPI0_Data[5]: 0v
ULPI0_Data[6]: 1v
ULPI0_Data[7]: 1v

  These levels do not change, which is a stable continuous voltage waveform. I think only enable the case of the clock, should be idle state, idle state is Low? Is there a problem here?

 

  Second, is the voltage at ULPI0_Data[6:7] a normal voltage?

  All of these outputs are LOW until the clock is enabled.

  Looking forward to your help!

 

H-chips

0 Kudos
Reply
1 Solution
3,174 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

MCU drives TX CMD on data lines but NXT is driven by PHY, so if TX CMD is proper, rather consult USB3340 datasheet for detailed info.

BR, Petr

View solution in original post

0 Kudos
Reply
5 Replies
3,213 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

ULPI0_Data are bidirectional pins, question could be who is driving it. 1V does not seems to be correct voltage. Is there any device connected to ULPI interface? What about other signals (DIR, NXT, STP)?
The RM indicates DIR pin should have weak pull down enabled, so check that.

BR, Petr

 

0 Kudos
Reply
3,183 Views
H-chips
Contributor III
Hello, I have found that Data[6] and Data[7] are short-circuited, resulting in both performances of 1V.

But the new problem is that after sending the TXD CMD, the USB controller (USB3340) does not pull the NXT up. What are the possibilities?
0 Kudos
Reply
3,175 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

MCU drives TX CMD on data lines but NXT is driven by PHY, so if TX CMD is proper, rather consult USB3340 datasheet for detailed info.

BR, Petr

0 Kudos
Reply
3,127 Views
H-chips
Contributor III
Ok, thank you very much, I will check this topic.
0 Kudos
Reply
3,198 Views
H-chips
Contributor III
Thank you very much for your answer. I will check it over here.
0 Kudos
Reply