Quadrature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Quadrature

4,268 Views
zhang_ke_dong
Contributor I

When the eTimer module of MPC5744P decodes ABI orthogonally, there is a problem in reading the CNTR register value at low motor speed?

MPC5744P chip SDK3.0.3 How to set the comparison value to zero after CNTR reaches the comparison value?

Why is it longer when the motor Angle reaches 360° to 0°?

0 Kudos
Reply
2 Replies

4,235 Views
KaiRiek
Contributor I
I think your configuration ist correct. You just may have a problem with showing your measurement results. I guess your measurement sampling rate ist slow and does not fit the motor speed (which is ok). So you get undersampling which leads to your described behavior.
0 Kudos
Reply

4,257 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

there is a problem in reading the CNTR register value at low motor speed?

What do you mean by problem reading CNTR?

There is no restriction on reading CNTR register:

petervlna_0-1671692879332.png

Best regards,

Peter

 

0 Kudos
Reply