Problem getting started with MPC56xxS Software Graphics Library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem getting started with MPC56xxS Software Graphics Library

ソリューションへジャンプ
2,932件の閲覧回数
fieroluke
Contributor II

I am trying to flash some of the MPC56xxS Software Graphics Library (LibsV2_0R46) Lab exercises on my 5606S board, and I keep getting an error 18.

 

I removed the QSPI section from the LCF file, and the project compiles fine then, but programming fails with "Programming address $   Error - out of memory".

The erase works fine too.

 

A different (small) application flashes fine, so the board and processor are okay.

I'm using CW MPC56xx 2.9.

 

Does anyone have any hint as to what might be the cause for this?  I'm sure there's a simple explanation...

 

Oliver

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,641件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

There can be several reasons for “Error 18”. I have already met the following:

- your license for CodeWarrior was limited – check the restricted C-code and data size of your license.

- s-record file contains records that does not belong to flash – check the linker file if everything is ok.

- censored device. This is not your case for sure.

Regards,

Petr

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,641件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

There can be several reasons for “Error 18”. I have already met the following:

- your license for CodeWarrior was limited – check the restricted C-code and data size of your license.

- s-record file contains records that does not belong to flash – check the linker file if everything is ok.

- censored device. This is not your case for sure.

Regards,

Petr

0 件の賞賛
返信
2,641件の閲覧回数
fieroluke
Contributor II

Thanks, you are correct!

Turns out the license was indeed limited - at least the flash utility was, it's the 128K version.

I had assumed that a demo that only contained the lib and not much else would be within the 128K limit. It was not.

In any case, the error message was a bit misleading, a "feature not licensed" or "file exceeds 128K" would have been more meaningful than "error 18 - out of memory". Oh well.

I have to get the unlimited version now...

anyway, thanks again for your quick help!

0 件の賞賛
返信