Output Compare Interrupt Not Firing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Output Compare Interrupt Not Firing

4,181件の閲覧回数
robertwynn
Contributor I

I am using the TRK-MPC5634M board and Codewarrior to test an output compare.

I need to know when the OC is done, so I can check some other things.

eTPU->CHAN[0].SCR.B.CIS indicates that the interrupt has fired in the ETPU.

What am I missing in order to route the interrupt back to the processor?

Thanks

partial below
void main(void)
{
  init();
  test();
  while(1){};
}

void init(void)
{
  etpuInit();
  INTC_InitINTCInterrupts();
  INTC_InstallINTCInterruptHandler(etpu_0_ISR, 68, 5); // interrupt for ETPU_0  (68)
 
  fs_etpu_interrupt_enable(0);
  fs_etpu_clear_chan_interrupt_flag(0);
 
  INTC .CPR.R = 0;
  asm(" wrteei 1");
}

void test(void)
{
  SIU .GPDO[ETPU_A1_PIN].R ^= 1; // toggle output so I can see start

  fs_etpu_oc_init_immed(0,               // channel
      FS_ETPU_PRIORITY_HIGH,             // priority
      FS_OC_MATCH_TCR1,                  // match timebase
      1000,                              // offset1
      FS_ETPU_OC_PIN_HIGH_CAPTURE_TCR1,  // pin action
      10000,                             // offset2
      FS_ETPU_OC_PIN_LOW_CAPTURE_TCR1,   // pin action
      FS_ETPU_OC_INIT_PIN_NO_CHANGE);    // init pin    

  fs_etpu_clear_chan_interrupt_flag(0);
}

void etpu_0_ISR(void)
{
  SIU .GPDO[ETPU_A1_PIN ].R ^= 1;
  fs_etpu_clear_chan_interrupt_flag(0);
}

0 件の賞賛
返信
9 返答(返信)

3,984件の閲覧回数
robertwynn
Contributor I

I finally figured out what I was missing. The default OC does not enable the interrupt.

If I add ETPU.CIER_A.B.CIE0=1 the interrupt fires at the end if the event. Just what I needed.

0 件の賞賛
返信

3,984件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't see anything obvious from this code snippet. OC function works fine in other aspects? And have you tried other interrupt sources (for instance PIT) to check whether you have properly working interrupts?

0 件の賞賛
返信

3,984件の閲覧回数
robertwynn
Contributor I

Other interrupts work fine. The OC works (i.e. the output toggles when it should). I just can't get the interrupt to fire.

0 件の賞賛
返信

3,984件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just tried it and it works fine on my side.

pastedImage_1.png

I can share example code if needed

0 件の賞賛
返信

3,984件の閲覧回数
robertwynn
Contributor I

Please share your code.

0 件の賞賛
返信

3,984件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am currently at home office without any hardware to check it but I believe I have attached the right code. Certain configuration in the main function, the rest configured with eTPU GCT, config file in the /src folder. Note that it is just raw state without any comments.

0 件の賞賛
返信

3,984件の閲覧回数
robertwynn
Contributor I

   I ran your code. The interrupt does fire, but only once. At power-up the OC and the interrupt fire, but if you reload the OC (change I made) the interrupt does not fire. I checked eTPU->CISR_A.B.CIS0 and it was still 1. I cleared it again (got 0) and the interrupt still did not fire again.

0 件の賞賛
返信

3,984件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is not supposed to.

If you need periodic pulses, use function QOM function:

https://www.nxp.com/docs/en/application-note/AN2857.pdf 

0 件の賞賛
返信

3,984件の閲覧回数
robertwynn
Contributor I

I will look at that. What I want is a way to detect when the OC is done. (without polling it), so I can load it with the next event.

I guess I don't understand the purpose/implementation of the OC interrupt.

0 件の賞賛
返信