Os Generation Failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Os Generation Failure

2,545 次查看
Taresh
Contributor I

Taresh_0-1749891324619.pngTaresh_0-1749891324619.png

Hello, i am getting the above highlighted error during generation of OS module.
Seems like generator is taking wrong Command.

Please let me know if any fix for this.


Thanks

0 项奖励
回复
3 回复数

2,500 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Which version of Tresos do you use?

Could you try latest version r29 ?

Could you share more details on the issue?

best regards,

Peter

0 项奖励
回复

2,485 次查看
Taresh
Contributor I

Hello, 

i am using tresos version 29 and using sample application from MPC574XG_MCAL4_0_RTM_1_0_5 which has both MCAL PLUS OS sample application.
but initially Plugin were missing for OS in plugin folder. i added manually as shown in below image after that OS module got reflected in tresos and when i was trying to generate the  module in tresos i am the error as seen in the last Images. 

Taresh_0-1750079644854.pngTaresh_0-1750079644854.png

Taresh_1-1750080408142.pngTaresh_1-1750080408142.png

 

0 项奖励
回复

2,462 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have just tried the sample SC2 from OS pluggin.

I worked with 0 errors right after installation and import of SC2.

The files were generated successfully.

There must be some issue on your side as here it is working correctly.

Maybe try reinstalling the OS plugin so the paths will be set to default to the OS plagin in tresos.

Best regards,

Peter

0 项奖励
回复