Os Generation Failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Os Generation Failure

2,415件の閲覧回数
Taresh
Contributor I

Taresh_0-1749891324619.pngTaresh_0-1749891324619.png

Hello, i am getting the above highlighted error during generation of OS module.
Seems like generator is taking wrong Command.

Please let me know if any fix for this.


Thanks

0 件の賞賛
返信
3 返答(返信)

2,370件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Which version of Tresos do you use?

Could you try latest version r29 ?

Could you share more details on the issue?

best regards,

Peter

0 件の賞賛
返信

2,355件の閲覧回数
Taresh
Contributor I

Hello, 

i am using tresos version 29 and using sample application from MPC574XG_MCAL4_0_RTM_1_0_5 which has both MCAL PLUS OS sample application.
but initially Plugin were missing for OS in plugin folder. i added manually as shown in below image after that OS module got reflected in tresos and when i was trying to generate the  module in tresos i am the error as seen in the last Images. 

Taresh_0-1750079644854.pngTaresh_0-1750079644854.png

Taresh_1-1750080408142.pngTaresh_1-1750080408142.png

 

0 件の賞賛
返信

2,332件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have just tried the sample SC2 from OS pluggin.

I worked with 0 errors right after installation and import of SC2.

The files were generated successfully.

There must be some issue on your side as here it is working correctly.

Maybe try reinstalling the OS plugin so the paths will be set to default to the OS plagin in tresos.

Best regards,

Peter

0 件の賞賛
返信