Nested macro opening within "[!ERROR]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Nested macro opening within "[!ERROR]

1,568件の閲覧回数
ma_cg
Contributor III

Greetings,

The previous problem description may have been inaccurate, my problem is not because the core file had to be modified and then the signature problem was incorrect.

When I configured devkit-mpc5748g using EB tresos27.1.0, MCAL, The corresponding MCAL links to https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=9653727

After the MCU module is configured, there is no problem in compiling. After the GPT module is added and configured, There came the "Parsing file "D:\EB tresos 27.1.0\EBtresosStudio_EBtresosStudio\plugins\Gpt_TS_T2D35M10I5R0/generate_PC/src/Gpt_Cfg.c (signed)", line "96"
[D:\EB tresos 27.1.0\EBtresosStudio_EBtresosStudio\plugins\Gpt_TS_T2D35M10I5R0/generate_PC/Gpt_VersionCheck_Src.m (signed):54]: Nested macro opening within
"[!ERROR]
"AUTOSAR release revision version number of the Basic Software Module Description ..." "

In this case, the message [!ERROR] does not close the loop correctly. Therefore, I modify the corresponding file as prompted, resulting in a signature problem. In summary, what I want to solve is the problem that [!ERROR] does not close the loop, and it is not necessary to modify the signature problem.    MPC574xB-C-G 

ma_cg_0-1723422406625.png

 

0 件の賞賛
返信
3 返答(返信)

1,552件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

When I configured devkit-mpc5748g using EB tresos27.1.0, MCAL, The corresponding MCAL links to https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&element=9653727

The link is private and generated just for you.

 

Not sure what is the issue. Looks like version conflict.

Could you export your project and share it with me so I can test it here?

Best regards,

Peter

1,547件の閲覧回数
ma_cg
Contributor III

Hello,

    MCAL is QM version of SW574XG_MCAL401-RTMC_SR-1.0.5.

The link is “https://nxp.flexnetoperations.com/control/frse/product?entitlementId=594560027&lineNum=1&authContact...

The arxml file of my EB configuration project is attached demo.arxml. The main modules used are Adc, Base, Dio, Gpt, Mcu, Port.

Looking forward to your reply

0 件の賞賛
返信

1,521件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I do not see any issues in your project nor any modules when I imported it.

Did you correctly export the project?

petervlna_0-1723532801798.png

 

Best regards,
Peter

0 件の賞賛
返信