Negative MPC5644A SPI hold times

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Negative MPC5644A SPI hold times

Jump to solution
1,197 Views
EAlepins
Contributor V

Hi,

 

In MPC5644A datasheet Rev 7, §3.17.8 "DSPI timing" mentions that the "Data Hold Time for Inputs" (10) is -4 ns and the "Data Hold Time for Outputs" (12) is -7.5 ns (VDDEH=3 –3.6 V). I am using CPOL=0 and CPHA=1 so I look at "Figure 24. DSPI classic SPI timing — master, CPHA = 1". What does the negative number mean?

 

a) The MPC5644A will keep the SOUT valid for 7,5 ns after the rising clock edge

OR

b) The MPC5644A will keep the SOUT valid up to 7,5 ns before the rising clock edge

 

Indeed, the figure is showing a period which is at the right of the clock's edge... Same question for inputs (10).

 

Thanks.

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
968 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

B is correct. Positive number means AFTER clock edge, negative number means BEFORE clock edge.

View solution in original post

0 Kudos
Reply
1 Reply
969 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

B is correct. Positive number means AFTER clock edge, negative number means BEFORE clock edge.

0 Kudos
Reply