Need help with eMIOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help with eMIOS

1,668件の閲覧回数
snehakalkhair
Contributor III


Hi,

I will be working on MPC5676R to design a controller for the BLDC motor.

I need help with the eMIOS.

I have the following question:

How is it connected with the SoC?

Is there any interface required with eMIOS and eTPU?

Are there any simulators on which i can practice programming the eMIOS?

Code Warrior can be used for eTPU only.

 

Please help.

ラベル(1)
1 返信

1,451件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is no simulator for eMIOS timer, as it is relatively simple peripheral in comparison to eTPU.

I could recommend AN2865, sections 18 and 19:

http://cache.nxp.com/files/32bit/doc/app_note/AN2865.pdf

Also following document could be useful to see (at least to know it exists):

http://cache.nxp.com/files/32bit/doc/app_note/EB651.pdf

I am not sure what would like to know SoC connection but if you ask about interconnection between eTPU and eMIOS, there is STAC bus and time bases synchronization:

  1. 21.3.5.3 STAC Interface
  2. 21.3.5.4 GTBE - Global Time Base Enable

If this question aims to pad to module routing then I would link to SIU module’s PCR registers configuring particular pins.