MPC5777C eTPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C eTPU

1,662 Views
liuhao11
Contributor I

Hi,

I was writing the ETPU-side code for the MPC5777C in BYTESCRAFT to detect the crankshaft signal. It doesn't work.

I have two questions:

1. Is the ETPU module of MPC5777C very different from the ETPU module of MPC5566?

2. Can the BYTECRAFT compiler be used for MPC5777C? The BYTECRAFT version is :

BYTECRAFT ETPU_C version 1.0.7.85

0 Kudos
Reply
1 Reply

1,654 Views
johndiener
Contributor IV

Hello Hanpeng,

With regards to #1 the MPC5777C eTPU has some differences, including the following:
- It has an eTPU2+ rather than eTPU1 - https://www.nxp.com/files-static/32bit/doc/ref_manual/ETPURMAD.pdf describes most of the differences. The eTPU2+ also supports up to 7 missing teeth and a few other small changes, beyond the eTPU2. However, the eTPU2+ is backwards compatible with eTPU1, so code compiled for older targets (say MPC5566 eTPU1) can work.
- The MPC5777C eTPU-AB module has more code and data memory than available on the MPC5566. It also has an eTPU-C module. And of course it can run at quite a bit higher frequency (up to 240MHz on some versions).

For #2 the basic answer is yes, since it can at the very least output eTPU1 code. But I believe the ByteCraft company no longer exists and thus the tool is probably unsupported. Here's another take from an older Community question on this topic: https://community.nxp.com/t5/MPC5xxx/Byte-Craft-eTPU-Compiler/m-p/652673.

John Diener
0 Kudos
Reply