MPC5777C FlexCAN Rx/Tx issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C FlexCAN Rx/Tx issue

4,949件の閲覧回数
beliyd
Contributor I

Hi!

I am trying to use FlexCAN on MPC5777C-516DS board without motherboard. So, I use DB9  (connected to GPIO[83] and GPIO[84] pins of MPC5777C)  to connect with other CAN interface device for test communication. Jumpers on MPC5777C-516DS: J506 1-2, 4-5; j507 1-3, 2-4.

  

I am referring example "Example-MPC5777C-FlexCAN-simpleTXRX-ECCdisabled-GHS616" (but work only with FlexCAN_A which connected to DB9). After upload the program I have next scenario:

- FlexCAN_A_Init() - successful;

- Trying to send 1 byte, ext. frame with CANA_TransmitMsg();

- Can not pass endless loop "while ( CAN_A.IFLAG1.B.BUF31TO8I  == 0)"

- Look at Error and Status 1 register (CAN_ESR1). It have 0x4036 value (Buss off, Bit0 error).

I checked up physical connection and signals on CAN bus:

- physical connection is ok;

- when I send 1 byte from MPC5777C-516D I have some signals on CNTXA line (attachment "CANbus_CNTXA.jpg"), but have no signal on CAN bus after MC33908LAE transceiver. 

- when I send 1 byte from my other CAN interface device to MPC5777C-516D, I have signals on CAN bus and the similar signal on CNRXA line (attachment "CANbus_CNRXA.jpg"). But CAN interface device reports an timeout error (like it is only 1 device on CAN bus).

Please suggest what kind of problem it can be.

Thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,729件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems the CAN transmitter is disabled, but it should be in normal mode if the SBC is put into Debug mode.

BR, Petr

0 件の賞賛
返信

4,729件の閲覧回数
beliyd
Contributor I

Hi, Petr!

Do you mean CAN transmitter "MC33908LAE" (placed on MPC5777C-516D) is disabled?

0 件の賞賛
返信