MPC5777C FEC Module Cannot connect to other device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C FEC Module Cannot connect to other device

1,095件の閲覧回数
lukezhang
Contributor III

Hi,

I'm trying to implement the ethernet module (FEC) using MPC5777c 516DS and MPC57xx Motherboard. I'm choosing RMII mode I'm referring the example code from AN4577 and the MPC5777M FEC example.

I used 2 ways to test it:

1. I'm using an external RJ45 loopback tester with TX and RX connect together and plug it in. The module works fine and the receiver can receive what the transmitter sends. The activity LED blinking but the link LED never turn on.

2. This time I connected 2 motherboards together with an Ethernet cable, both of chips program with the same code. But they are not communicate with each other, both stuck at isConnected(), which is used for checking "Link Status" bit and my link status bit is always 0.

Here's the function of isConnected()

int16_t isConnected()
{
   #if USE_LOOPBACK
   return 1;
   #endif
   

   uint16_t data;
   int16_t result = 0;

   if (miiRead(0x0001, &data))
      result = (data & 0x0004) ? 1 : 0;

     

   return result;
}

My hardware jumper configuration is:

  • 516DS:

      J25   - 12

      J524 - 12

      J510 - 23

      J26   - 23

  • Motherboard:

      J61 - 12

      J63 - 23

The code I'm referring is from 

Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP PHY This link. 

Thanks, 

Luke

タグ(2)
0 件の賞賛
返信
0 返答(返信)