MPC5777C Address lines of EBI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C Address lines of EBI

ソリューションへジャンプ
757件の閲覧回数
prathapvc
Contributor III

Does MPC5777C device offers 23 address lines in non-multiplexed mode?

When non-multiplexed mode has been choosen, bits 9-30 will be reflected on the external bus D_ADD [9:30]. There is 22 address line thus maximum memory size is 8Mbytes (=2^23 because of 16-bit data bus and so D_ADD31 is not used) per chip select.

1 解決策
648件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.

元の投稿で解決策を見る

2 返答(返信)
648件の閲覧回数
prathapvc
Contributor III

ok thank you

0 件の賞賛
返信
649件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.