MPC5777C Address lines of EBI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C Address lines of EBI

Jump to solution
731 Views
prathapvc
Contributor III

Does MPC5777C device offers 23 address lines in non-multiplexed mode?

When non-multiplexed mode has been choosen, bits 9-30 will be reflected on the external bus D_ADD [9:30]. There is 22 address line thus maximum memory size is 8Mbytes (=2^23 because of 16-bit data bus and so D_ADD31 is not used) per chip select.

1 Solution
622 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.

View solution in original post

2 Replies
622 Views
prathapvc
Contributor III

ok thank you

0 Kudos
Reply
623 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, 22 address lines. ADD31 is basically replaced by two byte strobe lines because 16-bit data port.