MPC5775K FLEXRAY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5775K FLEXRAY

1,261件の閲覧回数
ronliu
Contributor IV

Dear All,

I'm now working with MPC5775K. Could you please share me some example code of  FlexRay module?

Thanks a lot !

Best regards,

Ron

ラベル(1)
タグ(2)
2 返答(返信)

937件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Ron,

unfortunately we do not have any Flexray example, but there are two possibilities. First one is AUTOSAR OS and Flexray MCAL driver.

AUTOSAR Software Solutions|NXP

Second one is driver from Vector.

Solutions for FlexRay Networking

But both drivers are under license.

Regards,

Martin

0 件の賞賛
返信

937件の閲覧回数
clementchassagn
Contributor II

That's so sad to hear that :smileyhappy:

We contacted Vector, their FlexRay driver is AUTOSAR flavored and also AUTOSAR licensed (which means: reserved to worldwide recognized actors of the automotive industry). In short, there is only one FlexRay implementation, and it is not open to other industries :smileysad:

If the situation changed since last year, we may still be interested in a vanilla implementation of the FlexRay stack, even non-free...