[MPC5775E] Non linear eQADC conversion result issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MPC5775E] Non linear eQADC conversion result issue

865件の閲覧回数
AllGdC
Contributor I

Hi,

I am conducting a simple Analog-to-Digital conversion test on the MPC5775E and have observed nonlinear behavior in the eQADC conversion results.

Test Description:

  • Pins Tested: AN25 and AN32
  • Sampling: eQADC0 and eQADC1 sampling at 30 kHz
  • Input Signal: A 0.5 V to 4.5 V sawtooth waveform at 0.1 Hz generated using a signal generator
  • Setup: AN25 and AN32 are directly connected to the signal generator

Observations:

The conversion results are plotted in the attached graph, alongside an approximation line for reference. The data shows a clear nonlinear deviation from the expected values.
Nonlinear eQADC result conversionNonlinear eQADC result conversion

 

Result conversion error to line approximationResult conversion error to line approximation

 

  • The maximum conversion error is approximately 70 (in a 14-bit range) when compared to the approximation line, as shown in the second figure.
  • This nonlinear behavior persists regardless of using the calibration feature. Notably, the sampled voltages at 25% and 75% of the input signal range appear accurate.

Question:

Could this nonlinear behavior be attributed to a specific hardware or software configuration? Are there any known limitations or additional settings required to address this issue?

 

Thank you,

0 件の賞賛
返信
1 返信

839件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is interesting but it does not fit to eQADC validation results.

Could you specify used calibration routines? I could point out following example code:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-eQADC-Simple-Calibration-GHS714...

 

0 件の賞賛
返信