MPC5775B MCAL Integration with S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5775B MCAL Integration with S32DS

2,416 次查看
Lasya
Contributor II

Hi,

I am currently trying to integrate MCAL (Both generated and static ) with s32DS. I took S32K344_MCAL_Integrate_with_S32DS.pdf as reference and trying to integrate MPC5775B MCAL with S32DS. I found that startup and linker are to be deleted and use the files that are provided by MCAL (Provided screenshot for the same) . Unfortunately I don't find any startup file in the installed MCAL neither I found the platform folder. Couple you please help me resolve the issue at the earliest.

Attaching the reference doc as well and also the folder structure of installed MCAL.

Lasya_0-1743886811250.png

 

0 项奖励
回复
3 回复数

2,396 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lasya 
The startup files are not part of AUTOSAR MCAL. In the standard release, usually from RTM version, our Autosar MCAL package may include a sample integration application containing an example of startup file. However that is only a sample code, you can use that as a reference. The sample application is included in version 1.0.0 and you can find the startup files here after installation:
c:\NXP\AUTOSAR\MPC5777C_MCAL4_3_RTM_1_0_0\MPC5777C_MCAL4_3_RTM_1_0_0_Sample_Application\eclipse\plugins\PlatformIntegration_TS_T2D41M10I0R0\src\startup\
There's also user manual for the application which explains how to make it working:
c:\NXP\AUTOSAR\MPC5777C_MCAL4_3_RTM_1_0_0\MPC5777C_MCAL4_3_RTM_1_0_0_Sample_Application\eclipse\plugins\PlatformIntegration_TS_T2D41M10I0R0\doc\AUTOSAR_MCAL_SA_UM.pdf
Also notice that only Windriver and GHS compilers were tested:

lukaszadrapa_0-1744002749066.png

Regards,
Lukas

0 项奖励
回复

2,387 次查看
Lasya
Contributor II

Hi @lukaszadrapa ,

 

Thanks for the reply. I am currently using MPC5777C_MCAL4_0_RTM_1_0_2 for MPC5775B MCU. Can you help me out with this MCAL package. I am not able to find out the PlatformIntegration_TS_T2D41M10I0R0 folder to find the startup file. Kindly help me with this version of MCAL

标记 (1)
0 项奖励
回复

2,383 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

The sample application is usually available in first RTM version, not in minor updates. As I wrote, it can be found in 1.0.0. Just download this version.

0 项奖励
回复